From our HVLS, large diameter ceiling fan, to our circulators, these fans are designed to effectively improve air circulation in commerical and industrial spaces for maximum comfort.
Indicates the space relationships of windings and changing values of the recurring cycles of AC voltages and currents. The most common power supplies are either single- or three-phase.
The force that causes a current to flow in an electrical circuit. The voltage of a motor is usually determined by the supply to which it is attached. NEMA requires that motor be able to carry its rated horsepower at nameplate voltage plus or minus 1% al