Provide localized air direction and circulation where required.
Air circulators and mancooler fans provide localized air direction and circulation where required. Several mounting arrangements offer maximum directional flexibility and ease of mounting.
Indicates the space relationships of windings and changing values of the recurring cycles of AC voltages and currents. The most common power supplies are either single- or three-phase.
The force that causes a current to flow in an electrical circuit. The voltage of a motor is usually determined by the supply to which it is attached. NEMA requires that motor be able to carry its rated horsepower at nameplate voltage plus or minus 1% al